Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 38
The general purpose timers feature a total of 8 capture inputs, 4 external match outputs, and can act in counter or timer modes. Selected timer events can selectively generate DMA requests allowing for timed memory-to-memory transfers. The Watchdog Timer (WDT) function can be enabled by software but requires a hardware reset or a Watchdog reset/interrupt to be disabled. The WDT can also be used in Deep Sleep mode when using the IRC as the clock source. A debug mode is also provided wherein the watchdog can just interrupt the core instead of a full blown reset. The image on the right shows the different clock sources for the watchdog.
PTM Veröffentlicht am: