Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Slide 58 Product List
LPC1700 Microcontroller Slide 17
The booting process in the LPC1700 is similar to the LPC2000 family. The chip offers two ways to program the flash. The first way is In-System programming (ISP) which entails programming or reprogramming the on-chip flash memory using the boot loader software and UART0 serial port. This can be done when the part resides in the end-user board. The second way is In-Application Programming (IAP) which is the process of performing erase and write operations in the on-chip flash memory as directed by the end-user application code. If the flowchart is followed, it is possible to have two outcomes. If valid user code is present in the Flash, the bootloader will transfer code execution to internal memory. If no valid code exists, pin P2.10 is held low, the ISP mode is invoked, and the chip will look for ISP commands on the UART interface. Finally, the bootloader also provides Code Read Protection (CRP) that enables the application to apply different levels of security.
PTM Veröffentlicht am: