Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 15
The RTCC and DSWDT need a clock source to operate. When using the 31 kHz internal RC oscillator as a clock source, no external circuitry is required. For more timing accuracy, an external 32.768 kHz crystal can be connected to the microcontroller’s secondary oscillator pins (as shown in the example circuit). To achieve low-power consumption for Deep Sleep applications, the secondary oscillator has very low drive levels. The downside is increased sensitivity to rapidly changing signals in close proximity. Locate the crystal and capacitors as close to the microcontroller as possible and avoid routing signals, other than VSS and VDD, near the oscillator circuit.
PTM Veröffentlicht am: