Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 23
When the board is powered, a welcome screen is displayed and the board waits for the ‘Menu’ button to be pressed in order to load the bootloader. If the counter reaches 0, the last programmed application will be loaded. A MicroSD memory card can be inserted at any time. When it is detected by the MicroSD Bootloader, the MDD File System will be initialized, and the file structure will be displayed on the OLED. Please note, that only folders and HEX files will be displayed.
PTM Veröffentlicht am: