Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 20
Once the starter kit software is installed, connect the provided USB cable (A to mini-B) to any available USB port on the PC or powered hub, then to the starter kit at the mini-B receptacle on the application side of the board. The PC USB connection provides communication and power to the board. A MicroSD memory card, used to store the demo applications, may be connected to the starter kit at any time. If the cable is connected correctly, the green Power LED (D3) is lit. The OLED will display the “Microchip PIC18F Starter Kit” startup menu and the application processor will wait for the ‘Menu’ button to be pressed in order to load the MicroSD Bootloader.
PTM Veröffentlicht am: