Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 19
A major challenge in general purpose devices is providing the largest possible set of peripheral features while minimizing the conflict of features on I/O pins. Peripheral Pin Select allows peripherals to overlay each other. For example, mapping an interrupt on change input onto a UART receive pin allows the device to wake up from Sleep when a character is received. In addition, Peripheral Pin Select allows multiple pins to be used for a single output function, increasing the drive strength. For example, the Peripheral Pin Select can be used to multiplex the SPI communication lines with the PMP communication lines allowing for flexible usage of the I/O pins available on the part.
PTM Veröffentlicht am: