Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
EE-Slide5

Traditionally, 8-bit microcontrollers were challenged by the interface and program memory so that adding Ethernet for communication to the application was not feasible. There were two main reasons. First, adding Ethernet could be expensive. Integrated, single chip alternatives were not available. Second, Ethernet controller chips were designed originally for the PC industry and used a foreign interface increasing design complexity and consuming occupied board space. Finally, due to the number of I/O required to interface to the Ethernet controller, the number of available I/O for other control functions were severely limited. Another challenge was the program memory. Given that a few years ago, 8-bit microcontrollers were limited to 14-16Kbytes of program memory, TCP/IP stack footprints were simply too large for the available code space on the MCU.

PTM Veröffentlicht am: