Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
DF40-Slide12

In summary, Hirose’s DF40 series offers excellent space saving technology with high reliability. To provide feedback to the user, it features a clear click feeling when the connectors are mated. For added reliability of connection it also has an effective mating length of 0.45mm and enhanced self-alignment guide ribs. These features make the series ideal for applications that require space-saving, reliable, long lasting, flexible connections.

PTM Veröffentlicht am: