Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
SolutionSupport-Slide6

FT-MOD-4232HUB was selected as the I/O expansion module to bridge the USB port of the RPi2 to the peripheral components. The module is designed with an FT4232H USB-to-4-channel bridge IC. It is able to use one channel to convert USB to I2C for the sensors and another for converting USB to SPI for the display module, using a device mode known as MPSSE. Downstream USB ports available on the module are not used.

PTM Veröffentlicht am: