Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
SolutionSupport-Slide10

The Multi-Purpose-Synchronous-Serial-Engine (MPSSE) is a protocol defined by Bridgetek to enable synchronous serial interfaces of various standards, e.g. I2C, SPI, or JTAG. The MPSSE is the bus master, clocking data synchronised to a master clock. The FT4232H device used in this demonstration has two MPSSEs, allowing one to be used for communication with I2C devices and one for use with SPI devices.

PTM Veröffentlicht am: