Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
SolutionSupport-Slide16 Software

Not all programmers or developers are comfortable defining the data transfer at such a low level. To accommodate such users there is a wrapper library called LibMPSSE available which may simplify the programming for some. As can be seen from this slide the call SPI_InitChannel() which would enable the device for SPI data transfer is really no more than a wrapper for four D2xx calls which enable the MPSSE mode and define the pin idle state, clock frequency, and latency timer.

PTM Veröffentlicht am: