Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
attributes
In the ZigBee® Cluster Library, a cluster can support zero or more attributes, and attributes define the state of the application on that endpoint when clusters are commands. An example of this is an on/off light which has an attribute that describes whether the light is on or off. It is important to note that attributes are only used in a ZigBee Cluster Library and do not need to be defined in a manufacturer-specific application.
PTM Veröffentlicht am: