Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
2.4 ghz ch
Engineers may be concerned over the crowded 2.4GHz band. As shown in this slide, 802.11b, Bluetooth® and 802.15.4 are just a few of the solutions that share this channel. Note that the 802.11b spectrum occupancy is shown by the red arcs and the 802.15.4 channels are shown by the blue bars. While 802.15.4 utilizes interference avoidance techniques, such as listen before transmit, Wi-Fi environment channels 15, 20, 25, and 26 can be selected to reduce interference.
PTM Veröffentlicht am: