Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
cloud-kit-slide6

The XBee ZigBee Cloud Kit includes one XBee Gateway which connects ZigBee modules to the internet; one XBee ZigBee module; and one development board with a breadboard. The development board includes peripherals such as an audio buzzer, vibration motor, LEDs, switches and a potentiometer that a customer can interact with. The kit also includes basic prototyping components such as wires, LEDs, relay resistors and a temperature sensor. As part of the kit experience, Digi has included a sample web applicable which runs on the fully open sourced Heroku platform. The widgets are configurable and the web application is integrated with Device Cloud by Etherios™.

PTM Veröffentlicht am: