Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Cortex-M3 Introduction and Specific SAM3U Implementation Slide 5
The Cortex®-M3 used in the SAM3U has six code breakpoints and four general-purpose watchpoints, providing enough breakpoints for most cases of debugging. There are two debug interfaces: the JTAG and the Serial Wire Debug. The Cortex-M3 also allows live access to the core when the application is running, making it possible to read and write memory and to set or clear breakpoints on a running application.
PTM Veröffentlicht am: