Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Cortex-M3 Introduction and Specific SAM3U Implementation Slide 12
The table shown on this slide highlights the differences between the 144-pin and 100-pin versions of the SAM3U. The 144-pin version offers a 16-bit external bus interface with four chip select lines and an 8-bit multimedia card interface. In addition, both ADCs are upgraded to eight channels in the 144-pin version and one will be able to use up to ninety six GPIOs. The features which are not mentioned in this table are similar in both versions.
PTM Veröffentlicht am: