Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
ATmega128RFA1-Slide22

Microchip's Route Under MAC (RUM), with support for IPv6 and 6LoWPAN, is a highly flexible stack solution for low-power and low-cost wireless sensor network applications. Specifications are being defined by the Internet Engineering Task Force (IETF), while embedded IP-based solutions are being marketed by the IPSO Alliance (www.ipso-alliance.org). The Microchip IPv6/6LoWPAN implementation along with further information is available from www.atmel.com/6LoWPAN.

PTM Veröffentlicht am: