Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
IO-Connector-Slide2

Connectors do one of two jobs, they either connect boards together or equipment together. Typically attached to a length of cable, the I/O connector is the mechanism by which one device is physically connected to another where there may be some distance between the two. It is the physical interface of the equipment, providing an electrical pathway. How well the I/O interconnect 'bridge' is designed can positively or detrimentally affect the performance of a system.

PTM Veröffentlicht am: