Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
IO-Connector-Slide11

Connectors built using ribbon-style contacts differ from pin/socket method in two important ways. The illustration provided on this slide shows a cut-away of a mating pair of ribbon contacts. First, the contacts are pre-loaded in opposing directions, allowing for increased force. The resulting springiness in the contacts makes for a more reliable mating during operation. Second, the end of the ribbon style contact is retained inside an insulator. This greatly reduces the chance for a misaligned contact tip to catch and break against the outer face of the mating connector. Known as “pin stubbing”, this is quite common in pin-and-socket interfaces.

PTM Veröffentlicht am: