Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Sitara AM335x ARM Cortex -A8 Microprocessors Slide 9

Wi-Fi Direct devices have Wi-Fi’s traditional strengths of throughput and range. These devices work with legacy Wi-Fi CERTIFIED devices so virtually any application can be designed to run over the connection. The latest-generation security, WPA2, is easy to set up and protect with Wi-Fi Protected Setup™. It also has important new capabilities including: devices can find each other automatically, devices can see what other devices can do (e.g., print), support for multiple simultaneous connections (concurrent connections), separate security domains for infrastructure and direct connections, Enterprise-friendly device management, devices can connect to each other while staying connected to the Internet, and enhanced power management modes.

PTM Veröffentlicht am: