Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
MSP430 for Utility Metering Solutions Slide 14

The MSP430 eMeter roadmap and portfolio is illustrated in this figure. On the X-axis is time, on the Y-axis is integration. In the lower-left corner is a low end single-phase meter with ESP, which means it is a low cost, one-phase eMeter that customers can purchase and implement easily and quickly. The next step is single-phase with anti-tamper, then two-phase, three-phase, and three-phase with anti-tamper. Information regarding these products is available at www.ti.com/metering. In the red circles are two different products that are going to be released in the future. These are the new generation single-phase F67xx which is based on the MSP435xx platform, and a low cost metrology AFE which is a high accuracy analog front-end for applications such as sub-metering or as an analog front-end. Visit the TI metering website www.ti.com/metering for further details.

PTM Veröffentlicht am: