Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Solutions for PLC I/O Modules Slide 3

The diagram on this slide conceptualizes a typical programmable logic controller which can be segmented by I/O count and scan rates. They can also be classified as brick type versus modular PLCs. A small or brick PLC has a fixed number of connections for inputs and outputs. Modular PLCs (like the one shown here) have a chassis (also called a rack) into which are placed modules with different functions. The processor and selection of I/O modules is customized to fit the application. Several racks can be administered by a single processor, and may have thousands of inputs and outputs. A special high speed serial I/O link is used so that racks can be distributed away from the processor, reducing the wiring costs for large plants.

PTM Veröffentlicht am: