Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PHYTER Family Slide 8
The scope plots show the relationship between the transmit control on one PHY and the recovered receive data valid signal of a link partner connected by a short patch cable. The plot on the left shows a typical non-determinist (5*125 MHz clock uncertainty) 32 ns in the recovered signal exhibited by many PHYs. PHYTER products have both a low absolute latency and an architecture that minimizes the jitter of this critical parameter. The plot on the right shows the same measurement with PHYTER showing <3 ns of RX_CLK jitter.
PTM Veröffentlicht am: