Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
PHYTER Family Slide 11
Flexible port switching allows the two ports to be ‘ganged’ together through the multiplexers shown between the channel and the host ports. In this way, data can be shared between the channels to allow applications such as media conversion, redundancy and port ‘sniffing’ to be configured without external components or management. The application note referenced contains other example applications and details on how to configure this feature in the device.
PTM Veröffentlicht am: