Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Image of Texas Instruments Data Converter Basics the the

Data converters are the interface between analog and digital circuits. They are described by performance parameters and precision parameters. The performance parameters are determined by the sampling frequency and resolution. While, precision parameters are generally categorized in two ways: DC accuracy and dynamic performance. The DC accuracy specifications include DNL, INL, Offset Error, and Gain Error. The dynamic performance is categorized with SNR, THD, ENOB, and SFDR. To learn more about these parameter and data converters please visit http://dataconverter.ti.com.

PTM Veröffentlicht am: