Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Image of Texas Instruments Data Converter Basics

For a DAC, a DNL error of -1LSB implies that the output did not increase for an increasing input code. A DNL error of greater than - 1LSB implies that the device is non-monotonic. For an ADC a DNL error of greater than -1LSB implies that at least one code is missing, meaning that there is no analog voltage which will generate a particular code. Most manufacturers will include a “NO MISSING CODES” specification. A modern SAR A/D converter uses an array of capacitors and a comparator to determine the value of each bit in the conversion result. Variations of the individual capacitors will produce periodic fluctuations in the DNL data. These variations can be seen in DNL vs Code plots of a datasheet.

PTM Veröffentlicht am: