Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 25

There are many modes to start the scope, the digitizer. There is auto trigger, which is continuously triggering on internal time base, and normal triggering that is continuously triggering as long as a trigger condition is met. For example, it could be a voltage level. Another mode is the single shot trigger, which allows the user to arm the oscilloscope and take a single capture either through a remote command, or by pushing a button on a front panel. Also, it is possible to trigger on any of the four analog inputs or on the digital channels in a mixed signal environment. Lastly, there is the choice of an external trigger available.

PTM Veröffentlicht am: