Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Product List
Fundamentals of Oscilloscopes Slide 14

When looking at the waveform display, there are quite a few things being displayed. The first is the wave forms that have been captured, the measured signal. There is the ability to zoom the signal display. Math functions can be enabled, for example to create a second trace. There is the capability of making measurements, manual cursor measurements, statistics and etc. Lastly, there are set up buttons for setting up things such as the channel menu, triggering, the horizontal and vertical scales. These are all located right on the front panel of the display.

PTM Veröffentlicht am: