Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Eurostyle Terminal Blocks Slide 18

One final consideration for a terminal block is its user friendliness. That is where the options shown here come into play. For ease of wiring for the installers, circuit identification printed onto the terminal blocks may be needed. If there are multiple headers on a board and an installer wants to easily identify which plug mates to which header, additional colors may also be considered. Or finally, to eliminate installing terminal blocks on the PCB backwards, locating pins are also available.

PTM Veröffentlicht am: