Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
GWS500-Slide3

When in standby mode, the GWS500 draws less than 0.5W from the input, is 1U high and can operate over a wide temperature range of -25°C to 70°C - derating is required above 50°C. The unit is fully featured, which will be discussed in more detail in the following slides.

PTM Veröffentlicht am: