Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
STM32 Cortex-M3 32-bit Microcontrollers Slide 7

This graphic shows the performance of the Cortex-M3 core compared with the ARM7TDMI core and other 16-bit cores. Note that the Cortex-M3 core outperforms the ARM7TDMI and 16-bit cores at all clock frequencies. Additionally, the STM32 Cortex-M3 core can be clocked at high frequencies so the maximum available performance is much higher than the other cores.

PTM Veröffentlicht am: