Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
STM32 Cortex-M3 32-bit Microcontrollers Slide 6

The STM32 also includes an embedded interrupt controller to ensure deterministic behavior. This provides very quick interrupt response times so that inter-interrupt latency is as low as 6 cycles and fast wake up from low power modes. There are also significant debug improvements on the Cortex-M3 which include Serial Wire debug, two data watchpoints, and eight hardware breakpoints.

PTM Veröffentlicht am: