Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
open.Audio Algorithms and Hardware Slide 12

This is the software the user needs to run on their PC in order to enable the beamforming and sound localization algorithms. It is user friendly, with the ability to select the directivity of the beam forming and enable or disable the sound localization. The communication from the demo and the computer is based on a COM port via the USB connection.

PTM Veröffentlicht am: