Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
field instal
UTL is available with optional screw termination contacts to allow terminating the cable assembly to the connector in the field. Special crimp tooling or overmolding is eliminated and the length of the cable can be determined at the job site. The screw terminal contact is available in the 5-position UTL layout which also offers an additional snap together clamshell style backshell.
PTM Veröffentlicht am: