Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
safety qual
The highest priority for any electrical installation is to protect personnel from electrical shock hazard. Souriau-Sunbank by Eaton qualified the UTL series in accordance with the UL 1977 standard and also the IEC 61984 standard. The connector series can be engaged or disengaged during normal use when live or under power load. Designed with a first-mate, last-break contact, the mating is initiated on the designated ground line. In addition to this very important design feature, the UTL connector is also compliant with the latest environmental regulations such as RoHS and its Chinese equivalent. The series is also rated to the UL94-5VA flammability specification, which is a higher test with more stringent requirements than the UL94-V0 rating that other connector manufacturers typically offer.
PTM Veröffentlicht am: