Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Unmatched Noise Immunity Achieved in Four International Noise Tests Image of ROHM's EMARMOUR™ Noise Test Graphs
Shown here are the results of the four international noise tests. Unparalleled noise immunity was achieved in each of the tests for radio wave emission, near field immunity, BCI, and DPI. The radio wave emission, near field immunity, and BCI tests evaluate how much the output fluctuates in response to an input noise signal. ROHM’s op amps, indicated by the red lines, show a level of stability surpassing that of the competition. The DPI test on the lower right compares the amount of input power required to achieve an output fluctuation of 300 mV, making it clear that ROHM’s op amps, which require a larger amount of power to achieve a 300 mV output fluctuation, deliver significant advantages when compared to other products.
PTM Veröffentlicht am: