Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 19
Major application are the TV and VCR tuners as shown in the right upper diagram. Another application would be the generic front end, as shown in the left lower diagram. Possible positions would be the LNA and in the local oscillator. Key parameters for Varactor diodes are the C = ƒ(V) curve, which is the curve of Capacitance as a function of the reverse applied voltage, on wafer capacitance matching, and series resistance.
PTM Veröffentlicht am: