Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
RF Small Signal Products Part 2 Slide 13
How can we realize the previously discussed switch modes? Here we illustrate how to construct a Shunt SPDT switch using an ordinary PIN diode. The SPDT switch is used when high isolation is required. Lets have a look how this circuit functions in transmit state. D1 is reverse biased, open across Tx, low impedance at the antenna at a ¼ length away. D2 is forward biased, shorts Rx, and presents open-circuit to the antenna at a ¼ length away. The transmit insertion loss (IL) depends on both rD and Cd of the PIN diode. Isolation, however, depends on the forward impedance of the diode, that can be made very low, and consequently a high impedance at a ¼ length away. Remember that because of the ¼ length sections Insertion Loss (IL) and Isolation are frequency dependent.
PTM Veröffentlicht am: