Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Real Time Clocks Slide 24
The quartz crystals used for low frequency oscillators are usually from the type tuning fork. These display a bell shaped frequency versus temperature dependency. At room temperature the frequency is nominal. At lower or higher temperatures the frequency drops and thus the kept time will start to lag the real time. To achieve an average accuracy over a certain temperature range, the oscillator must be tuned higher at room temperature. The oscillator can be tuned by selecting the correct values for the oscillator capacitors. The parasitic capacitance of the PCB-layout must also be taken into account.
PTM Veröffentlicht am: