Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Real Time Clocks Slide 2
In order to measure elapsed time, a standard unit of measure and an instrument to count the units is needed; this is called a clock. An RTC is a clock which is incorporated in an electronic product that keeps track of time, even when the rest of the system is switched off. An RTC is based on a quartz oscillator running at 32.768 kHz, which provides the heartbeat of the clock. It is easy to derive a 1 Hz signal to keep track of seconds, minutes, hours, etc. in dedicated registers in the RTC.
PTM Veröffentlicht am: