Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 8
If more storage space than onboard flash can provide is needed, the NXP LPC2200 and LPC2400 series provide an external memory interface to address external NOR or NAND flash, SDRAM, and many other types of memory.  NXP’s external memory interface provides a full 32-bit memory interface, with 24 bit addressing capability and 4 chip selects.  As a side note, the SDRAM capability is limited to the LPC2400 series.  NXP has 8 and 16-bit memory busses available on certain products in these families if pin count is an issue or the external memory interface is being used as a parallel interface that doesn’t need a full 32-bit path.
PTM Veröffentlicht am: