Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Product List
Migrating from 8/16-bit MCUs to 32-bit ARMs Slide 16
This slide summarizes the key differences between the CISC and RISC architectures. The CISC architectures rarely have any pipelines while all of the ARM cores implement them with varying complexity. Additionally, the ability to operate in different modes significantly improves the ARM cores ability to respond to interrupts and enable deterministic responses. The ARM cores also support some backward compatibility to some instruction sets with the thumb instructions. However, these additional features and modes come at a slight increase in complexity with more registers to track.
PTM Veröffentlicht am: