Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
HowTo-Slide8

There are two ways to change the image on the OLED pushbutton switch. Users can change the image by pressing down on the OLED device or by programming a timing sequence into the attribute block. First, this slide will show developers how to program the Development Kit to change images by pressing down on the SmartSwitch device. When the switch is pressed, the controller checks the active attributes of the switch. If the address of switch #1 is not equal to 0000 the image will be displayed on SP1 and becomes the active attribute. If SP1 is 0000 there will be no changes to the display or attribute address. If switch #2 is not equal to 0000 the image is displayed on SP2 and becomes the active attribute. If SP2 is 0000 there will be no changes to the display or attribute address. Once the attributes are programmed select save attribute. The attributes will be saved in the same folder as the images.

PTM Veröffentlicht am: