Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
HowTo-Slide7

Once the images are prepared and saved in the folder, open the Universal Communicator and click batch picture located on the top menu bar. A window will appear like the one shown above. Select the switch type from the pull down menu, then click import batch. Locate the folder where the images are stored, select an image and click open. All the images in the folder will be loaded. Next, click edit attribute and a new window will appear. The name of all the images and their addresses are displayed. If the image name is clicked on, it will be displayed at the bottom of the screen. There are five attributes in front of each image name and address. Their values can be inputted or changed using HEX numbers. These five attributes are called Attribute Blocks and determine how the Development Kit will display and change images on the OLED SmartSwitch. The Universal Communicator displays the address for each image. Users will input or change the addresses and timers in the attribute block by double clicking on it. Even though the addresses and inputs are HEX numbers, the user does not need to know HEX to program a Development Kit. Once changes have been made click the check mark to accept the changes.

PTM Veröffentlicht am: