Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide35

Industrial applications are similar to low power electronic applications regarding MOV placement. Here, users can see that an MOV is placed across the incoming AC power line as usual before a sensitive load is reached such as this motor controller. It is assumed that the power input line has an appropriate overcurrent protection fuse or breaker located somewhere upstream. An additional MOV is used at the motor site to remove transients generated by the motor itself.

PTM Veröffentlicht am: