Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide27

The Littelfuse Industrial series MOV devices are typically designed into equipment that is exposed to high levels of line disturbance. Their physical size is larger than the others and several mounting approaches are used to enable easy installation and replacement. The disc technology used is the same as the smaller types. The industrial types are larger to allow for a higher level of current during a clamping event. All of the voltages routinely found in industry are available, beginning at 130VAC.

PTM Veröffentlicht am: