Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide9

This application shown here stresses the versatility of dual protocol transceivers. When implemented into industrial PCs (IPC) or programmable logic controllers (PLC), dual protocol transceivers can provide direct links to instruments and machines equipped with RS-232 or RS-485 interfaces. If however, networking of multiple equipment is required, dual protocol transceivers can be configured to level translators or interface converters. The following slides show three variants of level translators using the ISL33334, each serving a different interface purpose.

PTM Veröffentlicht am: