Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide10

Configuration1 adds long distance drive capability to an RS-232 channel by connecting the logic I/O of the RS-232 transceiver with the logic I/O of the RS-485 transceiver. The full-duplex structure of the RS-232 interface is maintained for the entire data link. However, since the enable pin of the RS-485 driver is fixed to Vcc potential, the driver remains active all the time. This type of level translator is therefore only suited for point-to-point data links.

PTM Veröffentlicht am: