Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
DigitalPower-Slide21

Shown on this slide is a Power Map rail block overview in the PowerNavigator. As can be seen, it provides a quick overview of the digital power monitor, including the rail name, which is customizable, if using more than one DPM in the system. It also displays the telemetry reading of voltage, current and power. An online/offline status indicator, the PMBus address and which channel is on display (primary or auxiliary), as well as the device name are provided. It also features a PMBus enable or disable. 

PTM Veröffentlicht am: