Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
barracuda customer benefits
The Barracuda series adheres to the latest one eighth brick and one quarter brick DOSA footprints. This series is fully forward and backward compatible providing flexibility to customers for existing and future designs. Using this footprint allows for migration from one package to another as the series evolves, mitigating risk and providing cost reduction options in the future. Address pins, data pins, a clock pin, and two configurable pins are digital pins added to the standard pins for digital versions of these converters. The standard trim pin is available, which is also configured. Parallel features are also offered to enable load sharing. This feature provides a precise forced output voltage load regulation droop characteristic. The output set point and droop slope are factory calibrated to ensure optimum matching of multiple modules and their individual load regulation characteristics.
PTM Veröffentlicht am: